跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What are available substitutes for 2SA1206 and 2SC1842 transistors?

Latest Updated:02/01/2008

Question:

Transistors 2SA1206 and 2SC1842 are shown in the application circuit example in the Data Sheet of the uPD8670A in the stage following the Vout pin. The distributor I contacted said that these products were phased-out products and were not available.
What substitutes are available?

Answer:

The 2SA1462 may be substituted for the 2SA1206 and the 2SC1623A for the 2SC1842, but the package as well as some of the ratings and characteristics differ. See the Data Sheet for details.
Suitable Products