跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

TPS-1 PROFINET 2.3 Conformance Class C Test Controller

Last Updated:06/01/2017

Question:

How do you test the TPS-1 with PROFINET 2.3 in regards to Conformance Class C? There are no corresponding PROFINET controllers available at the moment.

Answer:

Siemens controllers are used for Conformance Class C tests.

 

Suitable Products
TPS-1
  • 本文是否實用?