跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

TPS-1 Start-up Time Before Communications

Last Updated:06/01/2017

Question:

How much time does it take until the TPS-1 starts communication with a host CPU?

Answer:

It takes up to 300 ms until the TPS-1 is ready for communication with a host CPU.
Suitable Products
TPS-1
  • 本文是否實用?