跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is done if data pin number differs from Renesas’ and the other SRAM?

Latest Updated:03/16/2012

Question:

When replacing SRAM, what should I do if the data pin number differs between Renesas’ and the other manufacturer’s SRAM?

Answer:

It is not a problem. However, for x16bit configuration products, please separate the upper I/O (DQ0 to DQ7) and the lower I/O (DQ8 to DQ15).
Suitable Products
Power MOSFETs for General Switching
Power MOSFETs for Automobile use
Asynchronous SRAM