跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is an SRAM soft error?

Latest Updated:03/16/2012

Question:

What is an SRAM soft error?

Answer:

A soft error is a bit upset error. The device is not damaged permanently and will operate properly after data is rewritten. A soft error occurs when an alpha-particle or neutron hits the Si substrate, and the number of electrons absorbed to a memory cell exceeds the critical charge. The soft error rate increases as finer process is adopted, because it becomes more difficult to keep stored charge for data storage.
Suitable Products
Asynchronous SRAM