跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is there a lower cost flash version of the H8/3664 ?

Latest Updated:03/18/2009

Question:

Is there a lower cost flash version of the H8/3664 ?

Answer:

The H8/3670F ( 8 kbytes ) and the H8/3672F ( 16 kbytes ) are both pin compatible lower cost versions of the H8/3664F. To reduce cost they have a few features missing such as I2C and sub clock.
Suitable Products
H8/300H Tiny
  • 本文是否實用?