跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What units are used for reprogramming the Flash memory?

Latest Updated:03/01/2005

Question:

(Flash Memory)   The Flash memory is written to in byte units. What units are used for reprogramming? [2005/03/01]

Answer:

The erase unit determines the reprogramming unit for the Flash memory; this is the area unit specified in the erase/program area select bits.
Suitable Products
  • 本文是否實用?