跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Which pins are affected in their input/output voltage by PVcc?

Latest Updated:03/24/2009

Question:

Which pins are affected in their input/output voltage by PVcc (Power for input/output circuit) voltage (3.3V or 5V)?

Answer:

Answer
Suitable Products
SH-Ether
SH7616
SH7615