跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Which mode should be used to perform synchronous operation?

Latest Updated:03/24/2009

Question:

MTU has a maximum 12-phase PWM output in combination with synchronous operation. Which mode should be used to perform synchronous operation?

Answer:

MTU incorporates five channel timers consisting of channel 0-4. When performing 12-phase PWM output, set channel 0, 1, and 2 to PWM mode 2 and channel 3 and 4 to PWM mode 1. The output pins at this time are as follows;
channel 0 : PWM mode 2 : TIOC0A,TIOC0B,TIOC0C,TIOC0D
channel 1 : PWM mode 2 : TIOC1A,TIOC1B
channel 2 : PWM mode 2 : TIOC2A,TIOC2B
channel 3 : PWM mode 1 : TIOC3A,TIOC3C
channel 4 : PWM mode 1 : TIOC4A,TIOC4C
Suitable Products
SH7144, SH7145
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045