跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What would be the effect if mode setting change during LSI operation?

Latest Updated:03/23/2009

Question:

It is written in the hardware manual that you shouldn't change the mode pin setting during LSI operation, but if it is changed, what effects can result?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
SH7018
SH7011