跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What to do with Avref pins when the A/D converter of SH7206 is not used?

Latest Updated:03/23/2009

Question:

How should I do with the AVref pins when the A/D converter of SH7206 is not used?

Answer:

The Avref pin should be connected to the 3V power supply even when the A/D converter is not used.
Suitable Products
SH7206