跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the recommended PAD diameter?

Latest Updated:09/28/2009

Question:

What is the recommended PAD diameter?

Answer:

Please refer to SH7619 Group Hardware manual's Appendix (C.Package Dimensions).
SH7619 ball pitch is 0.8 mm. So the recommended PAD diameter is showed as 0.35 mm to 0.45 mm.
Suitable Products
SH7619
  • 本文是否實用?