跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the manual PAUSE frame transmitting processing flow?

Latest Updated:03/25/2009

Question:

What is the manual PAUSE frame transmitting processing flow?

Answer:

The manual PAUSE frame transmitting processing flow is as follows;

(1) Set the TE bit of EtherC mode register (ECMR) and DM bit to "1".

  TE = "1": Activates transmitting function
  DM = "1": Specifies whole duplex transfer system

(2) Set MP15-MP0 bit of the manual PAUSE frame setting register (MPR) to TIME parameter value of manual PAUSE frame.

The manual PAUSE frame is transmitted by writing in MPR register.

Suitable Products
SH7618