跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the difference between SH7618 and SH7618A?

Latest Updated:03/23/2009

Question:

What is the difference between SH7618 and SH7618A?

Answer:

SH7618A is the product that the SH7618's both cache capacity and the capacity of Ether MAC transmit and receive FIFO are increased.

There is no other difference in the other points.

See the table below for reference.

 

  SH7618 SH7618A
Cache capacity 4KB 16KB
Ether MAC transmit and receive FIFO capacity 256B for each 512B for each
Suitable Products
SH7618
  • 本文是否實用?