跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Should I write H'0000 directory to the TCNTx_5 register to clear?

Latest Updated:09/11/2012

Question:

When using the MTU2 as the external pulse width measurement function, there is no source the TCNTx_5 ("x" can be U, V or W) to be cleared. Should I write H'0000 directory to the TCNTx_5  register to clear?

Answer:

Correct. Write H'0000 directly to the TCNTx_5 to clear the register.
Suitable Products
SH7285, SH7286
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7124, SH7125
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086