跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is the initial value of weak keeper circuit "High" or "Low"?

Latest Updated:03/23/2009

Question:

Is the initial value of weak keeper circuit "High" or "Low"?

Answer:

It is undetermine whether the initial value of holding level in weak keeper circuit is "High" or "Low" .

To hold the level intention to weak keeper circuit, it is necessary to process pull-up and pull-down.

Suitable Products
SH7206
SH7619