跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is manual reset of WDT listed in flash memory mode transitions diagram?

Latest Updated:09/10/2007

Question:

Is manual reset of the WDT also included in the reset state listed in the flash memory mode transitions diagram?

Answer:

It means only the power-on reset state by the reset pin,does not include the MRES.
Suitable Products
SH7065
SH7058
SH7055
SH7047 Series
SH7018