Is it vital to clear module standby of peripheral to use after power-on?
Latest Updated:03/17/2011
Question:
Is it necessary to clear the module standby of peripheral modules to use after power-on?
Answer:
Yes, it is necessary to do so.
After power-on reset, most of peripheral modules are in module standby state (clock is not supplied to modules). So, you must clear the module standby of peripheral modules to use at first.
After power-on reset, most of peripheral modules are in module standby state (clock is not supplied to modules). So, you must clear the module standby of peripheral modules to use at first.
Suitable Products
SH7286 |
SH7285 |
SH7263 |
SH7262, SH7264 |
SH7261 |
SH7243 |
SH7214, SH7216 |
SH7211 |
SH7206 |
SH7203 |
SH7201 |
SH7124, SH7125 |
SH7147 |
SH7146, SH7149 |
SH7144, SH7145 |
SH7131, SH7132, SH7136, SH7137 |
SH7083, SH7084, SH7085, SH7086 |
SH7065 |
SH7047, SH7049, SH7105, SH7107, SH7109 |
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108 |