跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible to use Serial IO with FIFO (SIOF) as asynchronous serial?

Latest Updated:03/23/2009

Question:

Is it possible to use Serial IO with FIFO (SIOF) as asynchronous serial?

Answer:

No, it is impossible to use the Serial IO with FIF0 (SIOF) as asynchronous serial.
Please use Serial Communication Interface with FiFO (SCIF) or Serila Communication Interface (SCI), when using asynchronous serial.
Suitable Products
SH7727
SH7720