跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible to output the SCI synchronous clock continuously ?

Latest Updated:03/18/2009

Question:

Is it possible to output the SCI synchronous clock continuously ?

Answer:

The clock signal is only output during a send operation when using SCI internal clock. Therefore simultaneous send/receive operations are required to conduct a receive operation while using the internal clock.
Suitable Products
SH7144 Series
SH7047 Series
SH7046 Series
SH7040 Series