跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible that FWP of microcomputer is connected with the I/O port?

Latest Updated:03/25/2009

Question:

Is it possible that the FWP(FWE) pins of microcomputer with on-chip flash is connected with the I/O port, and control rewriting the flash with software?

Answer:

It is fundamentally possible.

However, FWP(FEW) pins are the pins to protect the incorrect write/erase to the on-chip flash with hardware. 

When switching FWP(FEW) pins by the I/O port control with software, it is possible that on-chip flash can be rewritten /erased unexpectedly because of false operation of CPU, software bugs, and so on. Therefore, please make a system design after examining it enough.

Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017