跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it likely for channels to transmit and receive data simultaneously?

Latest Updated:03/23/2009

Question:

When the Serial Communication Interface has several channels within a SuperH microcomputer, is it possible for each channel to transmit and receive the data simultaneously?

Answer:

Because the Serial Communication Interface within SuperH microcomputer has baud rate generator built-in each channel, this enables each channel to transmit and receive the data simultaneously.
Suitable Products
SH7065
SH7058
SH7055
SH7018
SH7011