跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is fractional portion 0.5 cycle equivalent to standard value 1/2tcyc?

Latest Updated:09/11/2012

Question:

The delay cycles of the CS assert and the CSn negate can be extended to 0.5 and 1.5 cycles respectively by the SW[1:0] bit and the HW[1:0] bit of the CSn space wait control register (CSnWCR).

  1. Is it correct to say that 2 cycles are added to the Th and Tf respectively when 2.5 cycles are set to the bits.
  2. Is the fractional portion of 0.5 cycles equivalent to the standard value of "1/2tcyc" for the address delay time1 (tAD1) and CS delay time1 (tCSD1)?

Answer:

  1. 2 cycles are added to the Th when 10:2.5 cycle is set to the SW[1:0] bit, and 2 cycles are added to the Tf  when 10:2.5 cycle is set to the HW[1:0] bit.
  2. As you mentioned.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086