跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can you explain more the multi function timer pulse unit 2 (MTU2)?

Latest Updated:03/26/2009

Question:

In the multi function timer pulse unit 2 (MTU2), what is the difference between the start of two or more channels simultaneously by timer start register (TSTR), and the start of two or more channels simultaneously by timer counter synchronous start register (TCSYSTR)?

Answer:

MTU2S and MTU2 can be started at the same time by using timer counter synchronous start register (TCSYSTR).
Suitable Products
SH7206
SH7124, SH7125
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086