跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are vender & product ID needed for developer that uses USB controller?

Latest Updated:03/23/2009

Question:

Are vender ID and product ID necessary for the developer to develop the product that uses the USB controller built into the SuperH microcomputer?

Answer:

When the USB product is developed, the customer (manufacturer) who sells it as end-products has to acquire vender ID. Product ID is a number that the customer can allocate in the product.

Renesas Electronics doesn't offer the allocation service of vender ID and product ID of USB so that the customers need to acquire vender ID from USB Implementers Forum (USB-IF) by themselves.

Suitable Products
SH7763
SH7760
SH7727
SH7720
SH7705
SH7641