跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Are there instructions when making reset signal based on WDTOVF?

Latest Updated:03/23/2009

Question:

System resets with the WDTOR signals are explained in the WDT chapter in the hardware manual. However, are there any instructions and directions for use when creating a reset signal based on WDTOVF signals?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055
SH7018