跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How many planes can handle display units (DU)?

Latest Updated:05/06/2016

Question:

How many planes can handle display units (DU)?

Answer:

DU0 and DU1 have a total of eight (8) planes (display planes), which can each handle image data. Moreover, it is possible to  mutually superpose up to 8 planes.
Suitable Products
RZ/G1M
RZ/G1E
RZ/G1N