跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the pin level when set to n-channel open drain output?

Latest Updated:01/23/2014

Question:

What is the pin level when set to n-channel open drain output?

Answer:

When the bit in the port output data register of the corresponding pin is 0, the level is low. When the bit is 1, it is open (Hi-Z).
Suitable Products
RX630
RX63N, RX631
RX210