跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What is the FCU-RAM area?

Latest Updated:06/20/2013

Question:

What is the FCU-RAM area?

Answer:

The FCU-RAM area is where a dedicated sequencer (FCU) for programming of the ROM (flash memory for code storage) and data flash (flash memory for data storage) operates.
For more information, please refer to the "ROM (Flash Memory for Code Storage)" and "Data Flash (Flash Memory for Data Storage)" chapters of the hardware manual.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G