跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Targeted needs of the new RX65N/RX651

Last Updated:11/13/2017

Question:

What needs are the target of new RX65N/RX651 MCUs ?

Answer:

The expansion of devices operating at the edge of the Industrial Internet of Things (IIoT) has increased system manufacturers’ need for secure network connectivity and reliability, including secure on-the-go firmware updates.
The new RX65N/RX651 devices support these evolving security and reprogramability needs, offering integrated TSIP, enhanced flash protection, and other technology advancements to create a secure and stable integration far above other solutions in the market, as proven by the Cryptographic Algorithm Validation (CAVP) communications.
Suitable Products
RX65N, RX651