跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Schmitt Trigger Input Terminal

Last Updated:06/08/2017

Question:

To check if a terminal is a Schmitt trigger input or not, where should I look in the user’s manual?

Answer:

For a Schmitt trigger input terminal, see “DC Characteristics” description in the “Electronics Characteristics” section of your user’s manual.

The Schmitt trigger input terminal is the terminal described in the Schmitt trigger input voltage item.
However, depending on the pins, there are some that are not Schmitt trigger input pins when the pin functions are switched.

Suitable Products
RX Family
  • 本文是否實用?