跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Running a Web Server on an RX MCU

Last Updated:06/08/2017

Question:

Is it possible to install a web server on an RX MCU board?

Answer:

Yes, you can.
Please review "RX Family TCP/IP for Embedded system M3S-T4-Tiny Introduction Guide Firmware Integration Technology" and "RX Family Web server using the embedded TCP/IP M3S-T4-Tiny Module Firmware Integration Technology" for more information on how to do this.
For an example, please see the sample program "RX Family Application example using the embedded TCP/IP M3S-T4-Tiny(DHCP/DNS/FTP/HTTP) Firmware Integration Technology".
Suitable Products
RX62N
RX63N
RX65N
RX64M
RX71M
  • 本文是否實用?