跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

New functions for secure network connection and reliability

Last Updated:11/13/2017

Question:

To realize secure network connection and reliability (including secure on-the-go firmware updates) , what kind of functions does the new RX65N/RX651 MCU have?

Answer:

Integrating the TSIP into the new RX65N/RX651 MCUs enables systems control engineers to realize high root-of-trust levels for the device operation through a combination of three new features:

o Protect encryption key by TSIP
o Integration of encryption hardware accelerators including AES, 3DES, SHA, and TRNG as part of TSIP
o Protect boot code by area of Flash

Suitable Products
RX65N, RX651