跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is it possible to use the FCU RAM area for a user program?

Latest Updated:06/20/2013

Question:

When not using the flash ROM programming function, is it possible to use the FCU RAM area for a user program?

Answer:

FCU RAM cannot be used as user RAM.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210