跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is hardware flow control in CTS and RTS pins supported?

Latest Updated:01/23/2014

Question:

Is hardware flow control using the asynchronous communication CTS and RTS pins supported?

Answer:

It is supported. However, because CTS and RTS share a pin, they cannot be used simultaneously.
Suitable Products
RX630
RX63N, RX631
RX210