跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

I'm not using BCLK. What should I set to SCKCR?

Latest Updated:06/20/2013

Question:

I'm not using BCLK. What should I set to SCKCR?

Answer:

Please set SCKCR as follows.
Set the external bus clock (BCLK) select bit so that ICLK >= BCLK.
Fix the BCLK output stop bit to 1 (high level).
Suitable Products
RX62N, RX621
RX610
RX63T