跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

How to use CMT interrupts?

Latest Updated:06/20/2013

Question:

I cannot use CMT interrupts.

Answer:

Check whether the settings of interrupt source priority register n (IPRn) of CMT0 to CMT3 are correct.
The IPRn of CMT0 to CMT3 are IPR004 to IPR007 (n is not the interrupt vector number).

- Interrupt source priority register n (IPRn) (n = 004 to 007)
- Interrupt request register m (IRm) (m = interrupt vector number (28 to 31))

Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111