跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Effect of Crystal Oscillation Variations

Last Updated:06/08/2017

Question:

The operating frequency exceeds the recommended operating conditions due to oscillation variations with the crystal.  Will this cause any problems?

Answer:

If the operational frequency is exceeded due to oscillation variations, it will not affect MCU operations.
Suitable Products
RX Family
  • 本文是否實用?