跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Can the ICLK be set to a frequency lower than PCLK and BCLK?

Latest Updated:05/27/2013

Question:

Can the system clock (ICLK) be set to a frequency lower than that of the peripheral module clock (PCLK) and external bus clock (BCLK)?

Answer:

The system clock (ICLK) be set to a frequency lower than that of the peripheral module clock (PCLK). However, please do not set a frequency lower than that of the external bus clock (BCLK).

Please see the System Clock Control Register (SCKCR) and Usage Notes sections in the Clock Generation Circuit chapter of the user's manual: hardware.

Suitable Products
RX62N, RX621
RX62T
RX610