跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(RX630, RX63N, RX631, RX210, RX220, X110, RX111) What types of resonator can be connected and what can you recommend?

Latest Updated:06/20/2013

Question:

What types of resonator can be connected?
And is there a recommended resonator?

Answer:

A crystal resonator can be used for the main clock oscillator.
There are no particular resonators that we recommend.
Suitable Products
RX62T
RX610
RX62G
RX63T