跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

(RX210) Module stop control register can't be set. Any special setting needed

Latest Updated:06/10/2013

Question:

The module stop control register cannot be set. Is any special setting required?

Answer:

This product has a register write protection function that protects important registers from being rewritten. To perform settings to a protected register, writing must first be enabled by the above function.

Please refer to the application note "Register Write Protection Setting Example" (R01AN1206EJ) for details on the register write protection function.

 

Suitable Products
RX210