跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What are cares at TTL input mode for terminal pins ?

Latest Updated:07/26/2016

Question:

What are cares at TTL input mode for terminal pins ?

Answer:

Shoot- through-current on input buffer may occur according to voltage of terminal pins (out-of range voltage for VIH and VIL : midpoint potential) even if it is Hi-level voltage of TTL mode.
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15