跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Arrhenius Model

Latest Updated:08/01/2005

Question:

Arrhenius Model

Answer:

Thermal stresses mostly affect the life of a semiconductor device, among electrical, thermal, and mechanical stresses. The Arrhenius chemical reaction theorem has been proved to be useful for estimating the dependency of the response speed on thermal stress, and this theorem is used to expect the life of a semiconductor device.

L = A•exp (Ea/k•T)
 
L: Life
A: Constant
Ea: Energy of activation [eV]
k: Boltzman constant (8.6159 × 10-5 [eV/K])
T: Absolute temperature [K]


For details, refer to the Review of Quality and Reliability Handbook.

Suitable Products
 
  • 本文是否實用?