跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

On-chip Peripheral Functions of RL78/G1D Used by Bluetooth Low Energy Protocol Stack

Last Updated:02/05/2018

Question:

Which on-chip peripheral functions of the RL78/G1D does the Bluetooth® Low Energy protocol stack use?

Answer:

For on-chip peripheral functions of the RL78/G1D that are used, please refer to "5.3 RL78/G1D Hardware Resources used by the BLE Software" of the Bluetooth® Low Energy Protocol Stack User’s Manual (R01UW0095).
https://www.renesas.com/search/keyword-search.html#q=R01UW0095&genre=document
Suitable Products
RL78/G1D
Bluetooth
  • 本文是否實用?