跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Implement of Bluetooth low energy Security Features

Last Updated:09/20/2017

Question:

Is there a simple implementation method to support Bluetooth low energy security features with the Bluetooth® Low Energy Protocol Stack?

Answer:

The sample program below incorporates Security Library (R01AN3777) in both sample programs for Central and Peripheral roles.  The security library also provides APIs to allow for easy use of the security features of the Bluetooth® Low Energy Protocol Stack. Again, this library is available for  both Central and Peripheral roles.  It can also be used for both Embedded and Modem configurations.

Bluetooth® low energy Protocol Stack Embedded Configuration Sample Program (R01AN3319)
https://www.renesas.com/search/keyword-search.html#q=R01AN3319&genre=tooldownload

Suitable Products
RL78/G1D
Bluetooth
  • 本文是否實用?