跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Technical conformity mark indication of Japan Radio Law of RL78/G1D module embedded products

Last Updated:09/20/2017

Question:

Can the technical conformity mark and others of the Japan Radio Law for the RL78/G1D module (RY 7011) be displayed on the housing of a product in which the module is incorporated internally?

Answer:

Since the revision of the Japanese Radio Law in 2014, it is now possible to display the technical standard conformity certification and others for the radio module on the housing of product embedded the radio module that was certified as conforming to the technical standards. Therefore it possible to display the technical standard conformity mark and others for the RL78/G1D module on the housing of a product that uses the RL78/G1D module.  
Suitable Products
RL78/G1D
Bluetooth
  • 本文是否實用?