跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Difference between IE-70000-PC-IF-B & IE-70000-PC-IF-C?

Latest Updated:12/01/2011

Question:

What is the difference between the following two interface boards?
IBM PC/AT-compatible ISA BUS Interface Board
- IE-70000-PC-IF-B
- IE-70000-PC-IF-C

Answer:

"-C" indicates that the interface board supports the NS type.
If you use other than the NS type, both interface boards can be used in the same way.
Suitable Products
V850 Family