跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

C Source Not Compiled Even After Modifying Header_e² studio

Last Updated:9/13/2017

Question:


I modified a header file which is referred from source code(s) in a project and then executed 'Build project.'
However, this does not initiate compilation of the source code(s) referring the header file.

Answer:

This occurs because the header file is located out of dependency scan of the project.
Please rebuild the project, or if you are sure of which source code(s) refers the header file, please compile the source files manually so that you can build the project.
To compile the source files manually, please select the desired source file(s) in Project Explorer and then select "Build Selected File(s)" from the context menu.
Suitable Products
e² studio
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 本文是否實用?