跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

What does this error W0511179 mean using CC-RL compiler for RL78?

Latest Updated:07/14/2015

Question:

I am using the CC-RL compiler for RL78 devices. I get the warning message below when I try to compile files. Why does this happen?

W0511179: The evaluation version is valid for the remaining number days.

Answer:

The message appears because you have not registered your license key for CC-RL. You have a 60-day trial period from first building, and your usage is not restricted over that period as it is a free evaluation copy. The message indicates how much of that period remains. After the trial period, the linkage size is restricted to 64 K or fewer bytes, and the MISRA-C checking function becomes unusable.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family