跳至主要內容
Knowledgebase
Home
Renesas Electronics Taiwan - Knowledgebase

Is there any advantage in using a divided memory model?

Latest Updated:05/18/2015

Question:

I am using the CC-RL compiler for RL78 devices. Is there any advantage in using a divided memory model?

Answer:

If you use the small model, the generated code will have 16-bit addresses.
If you know that there will be less than 64K of code and data in advance, the amount of code will be smaller than with the medium model.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family